Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Product List
KeyPad-Slide16

The Shore and Asker gages are commonly listed material properties (as hardness) on Gap Pad data sheets. The hardness value should not be confused with modulus or stress-strain behavior. Modulus and hardness do not necessarily correlate to one another. Modulus is the ratio of Stress and Strain. To understand the Gap Pad characteristics, one has to look beyond the hardness value and instead, compare the modulus among the Gap Pads instead.

PTM Veröffentlicht am: