Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Product List
KeyPad-Slide4

Thermal Conductivity is defined as the property of a material to conduct heat. Heat transfer occurs at a higher rate across materials of high thermal conductivity than across materials of low thermal conductivity. Variables include the time rate of heat flow, thickness, area, and change in temperature. A material’s thermal conductivity is temperature dependent. Typically, the thicker the gap to fill, the more significant it becomes for higher thermal conductivity (i.e. Gap Pads). Always note the test methods when comparing Thermal Conductivity for TIM (for example, ASTM D5470).

PTM Veröffentlicht am: