Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Product List
MS-162B-Slide10

Isolation is also important. Isolation is the amount of the signal going from the one PCB trace to the other PCB trace when in the mated condition. The lower the number, the better. The graph shows high isolation performance -20 dB or greater at 2 GHz and 12dB or greater at 10 GHz. This indicates the very good switching characteristics of the MS-162B as a coaxial switch.

PTM Veröffentlicht am: