Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Product List
MS-162B-Slide9

The previous slide showed the MS-162B in the un-mated condition. This slide shows the connectors in the mated condition with the signal going from the PCB trace to the plug side of the MS-162B. At 2 GHz the insertion loss is no more than -0.2 dB and a VSWR is no more than 1.2. Operating at 10 GHz the loss is still no more than -0.4 dB with a VSWR below 1.4. 

PTM Veröffentlicht am: