Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Product List
MS-162B-Slide7

Hirose is an environmentally aware company and the material selection for the MS-162B is no exception. In addition to meeting RoHS compliant directives, the MS-162B uses beryllium free copper alloy for springs, the insulator material is made halogen free by using a LCP (Liquid Crystal Polymer) material that does not contain bromide, which is typically used as a flame retardant. A plastic, polystyrene reel is used to eliminate the need for a paper/cardboard reel. 

PTM Veröffentlicht am: