Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Product List
MAX2870-Slide11

In the first scenario, the LO is set at 4745MHz, so the radio can select a channel at the 5745MHz RF carrier. This is called low side injection since the LO is a lower frequency than the desired carrier. The mixer output is a sum and difference of the RFIN and LO frequencies. The sum of the two frequencies is 10,490MHz. The IF filter is centered at 1000MHz. The 10,490MHz output is attenuated by the IF filter and is not passed to the VGA and ADC. The difference frequency is 1000MHz. The 1000MHz output is not attenuated by the IF filter so the ADC can capture the 20MHz wide channel present at 1000 MHz IF.

PTM Veröffentlicht am: