Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Product List
MAX2870-Slide14

When choosing a PLL frequency synthesizer, there are several key parameters to consider. Frequency range specifies the device RF output frequency range where the output is derived directly from the VCO or the divided output. Phase noise is a measure of short term frequency deviation from the ideal frequency due to random phase fluctuation. It is defined as the ratio of power measured in a 1Hz bandwidth to the total carrier power and expressed as dBc per Hz. Phase noise is specified at frequencies offset from the carrier. Common offset frequencies are 10kHz, 100kHz, 1MHz and 5MHz. It is common to measure single sideband phase noise. Fractional and Reference spurs are artifacts observed at the device RF output at an offset from the carrier frequency. Spurs are measured relative to the carrier. In an RF receiver down converter the spurious tones and phase noise will fold into the band of interest resulting in lower receiver sensitivity. An example will be shown later.

PTM Veröffentlicht am: