Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Product List
Clock and Data Distribution Products Part 2 Slide 4

Clock synthesizers are similar to clock generators, but clock synthesizers do not integrate a XTAL. An external crystal can be used as the input to a clock synthesizer. A clock signal can also be used. Clock synthesizers typically have configuration pins that allow the user to configure the PLL by selecting the appropriate multiplier. In the case of the NB3N501 shown at the bottom of the slide, there are 2 pins, S0 and S1 which each have 3 different levels: High, Low, or Floating. From these 2 pins, the user can select between 9 predefined multipliers as depicted in the table on the bottom right hand side of the slide. The internal PLL does not add any multiplication error, so the output frequency will have exactly the same precision as the external XTAL or as the input clock signal. The acceptable input and output levels; are device dependent, but generally, all common levels are supported.

PTM Veröffentlicht am: