Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Product List
General Purpose Motor Drivers in 3-15 Volt Range Slide 17

Shown on this slide are examples of how a motor driver can be used other than driving a motor. The first example is to control the movement of a solenoid. By providing current to a coil from the out pins of the driver, the iron core is moved. The user can change the direction of motion by changing the direction of current flow. This is how a valve can be opened and closed. Another application can be the electrolysis of water. The cathode and anode can be reversed by changing the direction of current flow.

PTM Veröffentlicht am: