Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Product List
General Purpose Motor Drivers in 3-15 Volt Range Slide 28

In summary, there are many applications for 3-15 VDC motor drivers, including security cameras, video projectors, toys, and valve control in water and gas applications. onsemi current products are developed on a DMOS process technology that employs a low Ron FET. A bipolar process would have to use a transistor, which consumes more power. Most of Sanyo’s 3-15 VDC motor drivers are monolithic ICs. There are four types of motor drivers, with different voltage levels and control methods. There are two control methods for the 3–5 VDC motor drivers; PWM current control uses internal control to do the chopping, whereas the full-on type is controlled externally for the chopping. For the 5–15 VDC motor drivers internal PWM control is used for high precision such as micro-stepping, the full-on method is used when simplicity and cost are the priorities.

PTM Veröffentlicht am: