Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Product List
General Purpose Motor Drivers in 3-15 Volt Range Slide 18

Most of Sanyo’s 3 to 15 VDC motor drivers are monolithic ICs. As the chart on this slide shows, there are four types of motor drivers, with different voltage levels and control methods. For lens drivers, the 3 – 5 VDC motor driver is recommended. There are two control methods for these products. The PWM control method uses internal control to do the chopping while the full-on type is controlled externally for the chopping. The same is true for the 5 – 15 VDC motor drivers. Internal PWM control is used when high precision is required like for micro-stepping. When simplicity and cost are the priorities, the full-on method is used.

PTM Veröffentlicht am: