Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Product List Associated Content
Overcurrent Protection with Two Adjustable Levels

Overcurrent protection (OCP) protects against inrush current on the load. ROHM IPD features two levels of current limit thresholds; one level that corresponds to the first initial inrush current spike during turn-on, and a second level for the following steady-state current level. Both of these OCP levels are adjustable. In addition, the masking time between OCP-1 and OCP-2 is also adjustable (as shown in the picture here), allowing great flexibility to provide the most optimal overcurrent protection for the system.

PTM Veröffentlicht am: