Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Product List
Si100x/1x ISM Transceiver Family Slide 12
Shown in this slide are several of the features of the ISM transceiver. One thing to note about the transceiver is that the functions are typically controlled by the hardware of the peripheral and do not require CPU overhead. The time division duplex transceiver provides the capability of the device to alternately transmit and receive data packets.
PTM Veröffentlicht am: