Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Product List
Si100x/1x ISM Transceiver Family Slide 21
There are two different methods for utilizing the wake-up timer (WUT) depending on whether the WUT interrupt is enabled or disabled. If the WUT interrupt is enabled then the nIRQ pin will go low when the timer expires. The chip will also change state to enable the 30MHz XTAL so that the microcontroller clock output is available for the microcontroller to use to process the interrupt. The other method of use is to not enable the WUT interrupt and use the WUT GPIO setting. In this mode of operation the chip will not change state until commanded by the microcontroller. The 32kHz RC oscillator provides an accurate time base compared to other non-crystal based oscillators and can be used to enable wake up events for the MCU as well.
PTM Veröffentlicht am: