Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Product List
Si100x/1x ISM Transceiver Family Slide 23
The presentation will now take a look at an example of an application where there is a set of sensor nodes that are required to take measurements and transmit the data to the control panel when asked. In many networks the control panel will send out a beacon frame to notify the node to send whatever data it may have collected. Each sensor node has its own time frame in which it looks for the beacon packet and transmits the data. This type of system requires the sensor to wake-up and listen for the beacon packet. It then has to respond and send the stored data to the control panel.
PTM Veröffentlicht am: