Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Product List
Silicon Carbide MOSFETs Slide 20

It must also be mentioned that Silicon Carbide MOSFETs are the only SiC transistor solution offering an intrinsic body diode with true SiC performance i.e. negligible reverse recovery charge. This is applicable in hard switching topologies often used in motor control. MOSFETs can be used in high power motor drives and other high power applications without any added complexity to the design.

PTM Veröffentlicht am: