Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Product List
Silicon Carbide MOSFETs Slide 6

The second SiC FET introduced by ST is the SCT20N120, a lower current, lower cost device as compared to the SCT30N120. It is rated at 20 A and 1200 V in the same HiP247 package that allows for operation up to 200°C. It is also in full production. The RDSON at 20 V gate drive is 200 mΩ at 25°C while only increasing to 225 mΩ at 125°C.

PTM Veröffentlicht am: