Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Product List
Silicon Carbide MOSFETs Slide 9

A case study will help clarify how dramatically an end application can be improved by designing with SiC MOSFETs over IGBTs. An internal evaluation has been preformed in a 5 kW boost converter using the SCT30N120 and the previously characterized 25 A IGBT. The investigation will look at the performance of each at 25 kHz, 100 kHz, and 125 kHz switching frequency. The remaining conditions will remain static as described in the slide here.

PTM Veröffentlicht am: