Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Product List
Small Motor Drivers Slide 15

The current generation of devices can implement both the power bridge and control logic in single ICs. The PowerSPIN family of devices includes dual H-Bridge driver ICs with various configurations of control logic. All of the devices in the family share some common characteristics. For the L620 series each MOS has a typical Rds ”on” of 0.3 Ohm. The lower current L622 series has a typical Rds ”on” of 0.7 Ohm. All of the devices implement the gate drive, level shift, thermal protection, cross conduction protection and logic inputs like we have discussed. The devices also implement an over current detection and protection that can be used to protect against shorts on the output.

PTM Veröffentlicht am: