Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Product List
Small Motor Drivers Slide 24

The integrated drivers we have discussed so far can drive motors up to 4 amps from supply voltages of 50V and below. For higher power motors, more current, a higher voltage, or both are needed. Such drive circuits are outside of the sweet spot that can effectively be done with fully integrated motor driver devices and we will need to move to discrete power MOS devices with gate drive circuits. In this configuration ST has a family of half bridge gate driver ICs designed to drive the gates of N-channel MOS devices for both the upper and lower device in the half H-bridge. When used in conjunction with the L6506, the L6384 provides a good solution for steppers.

PTM Veröffentlicht am: