Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Product List
Small Motor Drivers Slide 18

The L6207 adds the PWM current control for each bridge. Actually this is a fixed off time frequency modulation control that senses the voltage across the sense resistor and when it exceeds the reference, triggers a monostable that turns the bridge off for a fixed time set by the external RC network. The current control also has a blanking time built into the circuit that is set to ignore the switching noise at turn on that can sometimes fool the current control. All of the other features of the L6205 remain in the device.

PTM Veröffentlicht am: