Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Product List
Small Motor Drivers Slide 37

If the rotation needs to be reversed, then a provision must be made to reverse the direction of current flow in the motor. For cordless power tools this is typically done with a mechanical switch, for most other applications an H-bridge is typically used to drive the motor. For high power applications, gate driver ICs like the L6385 or L6386 that we have already seen, may be used to drive the gates of discrete Power MOS or IGBTs.

PTM Veröffentlicht am: