Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Product List
HVArc Guard Surface Mount MLCC Slide 13

Voltage multipliers can generate very high voltages with an inverter circuit that feeds a step-up transformer connected to the multiplier circuit. For example, the typical voltage multiplier shown here is simply a circuit comprised of HVArc Guard® capacitors and diodes that charge and discharge in alternating half cycles of the applied AC voltage. Cascading voltage doubler cells, as shown in the circuit, results in a high-voltage output. Applications for voltage multipliers include flyback converters (where a high voltage is produced from a low battery or supply voltage) in medical X-ray systems, air ionizers, and oscilloscopes, and instrumentation requiring a high-voltage power supply.

PTM Veröffentlicht am: