Maker.io main logo

3D Printed LED-Animation BMO

179

2025-05-16 | By Adafruit Industries

License: See Original Project 3D Printing Wearables

Courtesy of Adafruit

Guide by Ruiz Brothers

Overview

bmo_1

You can make your very own BMO with 3D Printing and DIY electronics. This guide will walk ‎you through the steps of 3D printing the parts, soldering the components, and assembling ‎this delightful electronic companion.‎

bmo_2

The mini 8x8 LED matrix makes an awesome head for BMO, programed to display several ‎fun and playful facial expressions. Program your own animation to make new faces, letters, ‎or totally mathematical expressions ;-)‎

3d_printing_hero2

This guide was written for the Gemma v2 board but can be done with either the Gemma v2 ‎or M0 Gemma. We recommend the Gemma M0 as it is easier to use and is more ‎compatible with modern computers!‎

Tools & Supplies

Parts

Prerequisite Guides:‎

3D Printing‎

3d_printing_3dparts_3

BMO's box enclosure, cover and limbs looks best printed in teal. A spool of teal-colored ‎ABS ranges from $30-50 depending on where you purchase it. ‎

Below is a small list of places to get filament. Make sure your filaments diameter size ‎matches your 3d printer. Most common size is 1.75mm and 3mm.‎

You can print BMO's buttons in different colored ABS or paint each piece. The buttons are ‎rather small, so you will need to make sure your build plate is clean and nicely leveled. ‎These parts are a bit difficult to print so make a few copies to make a batch of each. You ‎can do this in MakerWare by copying and pasting them.

The tolerances in the holes are optimized for ABS but should work with PLA. You can use an ‎x-acto knife in moderation to lose the tolerances to fit the components.‎

table_4

Download STLs

Painting BMO

If your 3D Print the buttons in different colored ABS, you only have to print BMO's letters on ‎the sides.

Use a fine brush and even out the bristles by trimming them with sharp scissors.

Black acrylic paint works best on ABS prints. Apply small portions of paint and spread it on ‎the surface of the raised letters on each side. Lightly dab on the edges to get a clean ‎finished look. If you accidentally mark outside the letters, quickly rinse it down with water ‎and try again. Let stand to dry for a few minutes.‎

paint_5

Circuit Diagram

diagram_6

This diagram uses the Gemma v2, but you can also use the Gemma M0 with the exact ‎same wiring!‎

Gemma + 8x8 LED Matrix

Using the GEMMA in this build allows us to plug in a rechargeable battery directly into the ‎JST port is directly on the board. GEMMA can be powered by USB but will need to have a ‎battery power source for portability.‎

  • VCC pin goes to VBAT

  • GND pin goes to GND

  • SCL pin goes to D2/A1

  • SDA pin goes to D0‎

3d_printing_complete-circuit_7

Prototyping

If your new to working with GEMMA, be sure to use a breadboard and jumper wires to ‎prototype. Use alligator clips to clip jumper wires to GEMMA. The 8x8 LED matrix ‎w/backpack will need header + pins soldered to the breakouts. Check out the Adafruit’s ‎guide to LED backpacks for more details.‎

Arduino Code

The Arduino code presented below works well on GEMMA v2.. But if you have an M0 board ‎you must use the CircuitPython code on the next page of this guide, no Arduino IDE ‎required!‎

If this is your first time using Gemma, work through the Introducing Gemma guide first; you ‎need to customize some settings in the Arduino IDE.

Be sure to check out Phil Burgess's space invader pendant guide for getting the source code ‎on to GEMMA properly.‎

Space Invaderz Guide

Once you have your GEMMA/Trinket profiles installed in your Adafruit Arduino IDE, copy this ‎code into a new sketch in Arduino and save it as matrix.ino.‎

Download File

Copy Code
// SPDX-FileCopyrightText: 2014 Phil Burgess for Adafruit Industries
//
// SPDX-License-Identifier: MIT
//
// Trinket/Gemma + LED matrix backpack jewelry.  Plays animated
// sequence on LED matrix.  Press reset button to display again,
// or add optional momentary button between pin #1 and +V.
// THERE IS NO ANIMATION DATA IN THIS SOURCE FILE, you should
// rarely need to change anything here.  EDIT anim.h INSTEAD.

#define BRIGHTNESS   12 // 0=min, 15=max
#define I2C_ADDR   0x70 // Edit if backpack A0/A1 jumpers set

#include <TinyWireM.h>
#include <avr/power.h>
#include <avr/sleep.h>
#include "bmo.h"       // Animation data is located here

static const uint8_t PROGMEM reorder[] = { // Column-reordering table
    0x00,0x40,0x20,0x60,0x10,0x50,0x30,0x70,0x08,0x48,0x28,0x68,0x18,0x58,0x38,0x78,
    0x04,0x44,0x24,0x64,0x14,0x54,0x34,0x74,0x0c,0x4c,0x2c,0x6c,0x1c,0x5c,0x3c,0x7c,
    0x02,0x42,0x22,0x62,0x12,0x52,0x32,0x72,0x0a,0x4a,0x2a,0x6a,0x1a,0x5a,0x3a,0x7a,
    0x06,0x46,0x26,0x66,0x16,0x56,0x36,0x76,0x0e,0x4e,0x2e,0x6e,0x1e,0x5e,0x3e,0x7e,
    0x01,0x41,0x21,0x61,0x11,0x51,0x31,0x71,0x09,0x49,0x29,0x69,0x19,0x59,0x39,0x79,
    0x05,0x45,0x25,0x65,0x15,0x55,0x35,0x75,0x0d,0x4d,0x2d,0x6d,0x1d,0x5d,0x3d,0x7d,
    0x03,0x43,0x23,0x63,0x13,0x53,0x33,0x73,0x0b,0x4b,0x2b,0x6b,0x1b,0x5b,0x3b,0x7b,
    0x07,0x47,0x27,0x67,0x17,0x57,0x37,0x77,0x0f,0x4f,0x2f,0x6f,0x1f,0x5f,0x3f,0x7f,
    0x80,0xc0,0xa0,0xe0,0x90,0xd0,0xb0,0xf0,0x88,0xc8,0xa8,0xe8,0x98,0xd8,0xb8,0xf8,
    0x84,0xc4,0xa4,0xe4,0x94,0xd4,0xb4,0xf4,0x8c,0xcc,0xac,0xec,0x9c,0xdc,0xbc,0xfc,
    0x82,0xc2,0xa2,0xe2,0x92,0xd2,0xb2,0xf2,0x8a,0xca,0xaa,0xea,0x9a,0xda,0xba,0xfa,
    0x86,0xc6,0xa6,0xe6,0x96,0xd6,0xb6,0xf6,0x8e,0xce,0xae,0xee,0x9e,0xde,0xbe,0xfe,
    0x81,0xc1,0xa1,0xe1,0x91,0xd1,0xb1,0xf1,0x89,0xc9,0xa9,0xe9,0x99,0xd9,0xb9,0xf9,
    0x85,0xc5,0xa5,0xe5,0x95,0xd5,0xb5,0xf5,0x8d,0xcd,0xad,0xed,0x9d,0xdd,0xbd,0xfd,
    0x83,0xc3,0xa3,0xe3,0x93,0xd3,0xb3,0xf3,0x8b,0xcb,0xab,0xeb,0x9b,0xdb,0xbb,0xfb,
    0x87,0xc7,0xa7,0xe7,0x97,0xd7,0xb7,0xf7,0x8f,0xcf,0xaf,0xef,0x9f,0xdf,0xbf,0xff };

void ledCmd(uint8_t x) { // Issue command to LED backback driver
  TinyWireM.beginTransmission(I2C_ADDR);
  TinyWireM.write(x);
  TinyWireM.endTransmission();
}

void clear(void) { // Clear display buffer
  TinyWireM.beginTransmission(I2C_ADDR);
  for(uint8_t i=0; i<17; i++) TinyWireM.write(0);
  TinyWireM.endTransmission();
}

void setup() {
  power_timer1_disable();    // Disable unused peripherals
  power_adc_disable();       // to save power
  PCMSK |= _BV(PCINT1);      // Set change mask for pin 1
  TinyWireM.begin();         // I2C init
  clear();                   // Blank display
  ledCmd(0x21);              // Turn on oscillator
  ledCmd(0xE0 | BRIGHTNESS); // Set brightness
  ledCmd(0x81);              // Display on, no blink
}

uint8_t rep = REPS;

void loop() {

  for(int i=0; i<sizeof(anim); i) { // For each frame...
    TinyWireM.beginTransmission(I2C_ADDR);
    TinyWireM.write(0);             // Start address
    for(uint8_t j=0; j<8; j++) {    // 8 rows...
      TinyWireM.write(pgm_read_byte(&reorder[pgm_read_byte(&anim[i++])]));
      TinyWireM.write(0);
    }
    TinyWireM.endTransmission();
    delay(pgm_read_byte(&anim[i++]) * 10);
  }

  if(!--rep) {             // If last cycle...
    ledCmd(0x20);          // LED matrix in standby mode
    GIMSK = _BV(PCIE);     // Enable pin change interrupt
    power_all_disable();   // All peripherals off
    set_sleep_mode(SLEEP_MODE_PWR_DOWN);
    sleep_enable();
    sei();                 // Keep interrupts disabled
    sleep_mode();          // Power down CPU (pin 1 will wake)
    // Execution resumes here on wake.
    GIMSK = 0;             // Disable pin change interrupt
    rep   = REPS;          // Reset animation counter
    power_timer0_enable(); // Re-enable timer
    power_usi_enable();    // Re-enable USI
    TinyWireM.begin();     // Re-init I2C
    clear();               // Blank display
    ledCmd(0x21);          // Re-enable matrix
  }
}

ISR(PCINT0_vect) {} // Button tap

View on GitHub

Create a new window and paste in the BMO animation code and save it as bmo.h in the ‎same directory as the matrix sketch.

You may have to remove the .ino extension that gets added to the bmo.h file making ‎it bmo.h.ino, remove that last .ino appending to just .h. Close the IDE and reopen it. The ‎matrix sketch should show the bmo.h file in a tab.

Go to the tools file menu and select the Adafruit Gemma 8MHz profile under the Board ‎drop down menu. Select USBTinyISP under the Programmer drop down in the tool file ‎menu.

Plug in a mini-USB cable to the Gemma and connect it to your computer. Wait until you see ‎a red blinking LED on the Gemma and then hit the left arrow icon button to upload the code.‎

If you get a message in the IDE "Done Uploading" the code successfully uploaded to the ‎GEMMA!‎

Download File

Copy Code
// SPDX-FileCopyrightText: 2014 Phil Burgess for Adafruit Industries
//
// SPDX-License-Identifier: MIT
//
// Animation data for Trinket/Gemma + LED matrix backpack jewelry. 
#define REPS 255 // Number of times to repeat the animation loop (1-255)
const uint8_t PROGMEM anim[] = {
  
  B11111111, // 1 frame
  B10011001,
  B10011001,
  B11111111,
  B10000001,
  B11000011,
  B11100111,
  B11111111,
  25, // 0.25 second delay
  
  B11111111, // 2 frame
  B10011001,
  B10011001,
  B11111111,
  B10111101,
  B10111101,
  B11000011,
  B11111111,
  25, // 0.25 second delay
  
  B11111111, // 3 frame
  B10011001,
  B10011001,
  B11111111,
  B10000001,
  B11000011,
  B11100111,
  B11111111,
  25, // 0.25 second delay
  
  B11111111, // 4 frame
  B10011001,
  B10011001,
  B11111111,
  B10111101,
  B10111101,
  B11000011,
  B11111111,
  25, // 0.25 second delay
  
  B11111111, // 5 frame
  B10011001,
  B10011001,
  B11111111,
  B11111111,
  B11111111,
  B10000001,
  B11111111,
  25, // 0.25 second delay
  
  B11111111, // 6 frame
  B10011001,
  B10011001,
  B11111111,
  B11100111,
  B11011011,
  B11100111,
  B11111111,
  25, // 0.25 second delay
  
  B11111111, // 7 frame
  B10111101,
  B00011000,
  B10111101,
  B11100111,
  B11011011,
  B11100111,
  B11111111,
  25, // 0.25 second delay
  
  B11111111, // 8 frame
  B11111111,
  B00011000,
  B11111111,
  B11100111,
  B11011011,
  B11100111,
  B11111111,
  25, // 0.25 second delay
  
  B11111111, // 9 frame
  B10111101,
  B00011000,
  B10111101,
  B11100111,
  B11011011,
  B11100111,
  B11111111,
  25, // 0.25 second delay
};
    

View on GitHub

Writing Custom LED Animations

Check out Phil Burgess's Space invader guide for a great break down on how to write your ‎own LED animations.‎

Animations Guide

Animation Tool for Adafruit 8x8 LED Matrix

Check out this awesome website for building letter-based LED animations. You simply click ‎on letters to build an animation which can then be out putted to animation data for the ‎Trinket/Gemma. It's awesome!‎

Mini 8x8 Animation Web Tool

CircuitPython Code

blinka_8

GEMMA M0 boards can run CircuitPython — a different approach to programming ‎compared to Arduino sketches. In fact, CircuitPython comes factory pre-loaded on ‎GEMMA M0. If you’ve overwritten it with an Arduino sketch or just want to learn the basics ‎of setting up and using CircuitPython, this is explained in the Adafruit GEMMA M0 guide.‎

These directions are specific to the “M0” GEMMA board. The GEMMA v2 with an 8-bit AVR ‎microcontroller doesn’t run CircuitPython…for those boards, use the Arduino sketch on the ‎‎“Arduino code” page of this guide.‎

Below is CircuitPython code that works similarly (though not exactly the same) as the ‎Arduino sketch shown on a prior page. To use this, plug the GEMMA M0 into USB…it should ‎show up on your computer as a small flash drive…then edit the file “code.py” with your ‎text editor of choice. Select and copy the code below and paste it into that file, entirely ‎replacing its contents (don’t mix it in with lingering bits of old code). When you save the ‎file, the code should start running almost immediately (if not, see notes at the bottom of ‎this page).‎

If GEMMA M0 doesn’t show up as a drive, follow the GEMMA M0 guide link above to ‎prepare the board for CircuitPython.‎

This code requires two additional libraries be installed:‎

  1. adafruit_circuitpython_ht16k33‎

  2. adafruit_bus_device

If you’ve just reloaded the board with CircuitPython, create the “lib” directory and then ‎download the Adafruit CircuitPython Bundle.‎

Due to pin differences on the Gemma M0 versus the Gemma v2 we are using D1 as the ‎optional touch-based reset. The onboard Gemma M0 switch and reset button will also ‎reset the animation.‎

Download Project Bundle

Copy Code
# SPDX-FileCopyrightText: 2014 Phil Burgess for Adafruit Industries
# SPDX-FileCopyrightText: 2018 Phil Burgess for Adafruit Industries
#
# SPDX-License-Identifier: MIT
#
# Trinket/Gemma + LED matrix backpack jewelry.  Plays animated
# sequence on LED matrix. Press reset button to display again.

import time
import adafruit_ht16k33.matrix
import board
import busio as io
import touchio

touch = touchio.TouchIn(board.D1)

i2c = io.I2C(board.SCL, board.SDA)
matrix = adafruit_ht16k33.matrix.Matrix8x8(i2c)

# pixels initializers
x_pix = y_pix = 8
x = y = 0
matrix.fill(0)
matrix.show()

# seconds to pause between frames
frame_delay = [.25, .25, .25, .25, .25, .25, .25, .25, .25, .25]

# counter for animation frames
frame_count = 0

# repeat entire animation multiple times
reps = 255
rep_count = reps

# animation bitmaps
animation = [
    # frame 1
    [[1, 1, 1, 1, 1, 1, 1, 1], [1, 0, 0, 1, 1, 0, 0, 1],
     [1, 0, 0, 1, 1, 0, 0, 1], [1, 1, 1, 1, 1, 1, 1, 1],
     [1, 0, 0, 0, 0, 0, 0, 1], [1, 1, 0, 0, 0, 0, 1, 1],
     [1, 1, 1, 0, 0, 1, 1, 1], [1, 1, 1, 1, 1, 1, 1, 1]],
    # frame 2
    [[1, 1, 1, 1, 1, 1, 1, 1], [1, 0, 0, 1, 1, 0, 0, 1],
     [1, 0, 0, 1, 1, 0, 0, 1], [1, 1, 1, 1, 1, 1, 1, 1],
     [1, 0, 1, 1, 1, 1, 0, 1], [1, 0, 1, 1, 1, 1, 0, 1],
     [1, 1, 0, 0, 0, 0, 1, 1], [1, 1, 1, 1, 1, 1, 1, 1]],
    # frame 3
    [[1, 1, 1, 1, 1, 1, 1, 1], [1, 0, 0, 1, 1, 0, 0, 1],
     [1, 0, 0, 1, 1, 0, 0, 1], [1, 1, 1, 1, 1, 1, 1, 1],
     [1, 0, 0, 0, 0, 0, 0, 1], [1, 1, 0, 0, 0, 0, 1, 1],
     [1, 1, 1, 0, 0, 1, 1, 1], [1, 1, 1, 1, 1, 1, 1, 1]],
    # frame 4
    [[1, 1, 1, 1, 1, 1, 1, 1], [1, 0, 0, 1, 1, 0, 0, 1],
     [1, 0, 0, 1, 1, 0, 0, 1], [1, 1, 1, 1, 1, 1, 1, 1],
     [1, 0, 1, 1, 1, 1, 0, 1], [1, 0, 1, 1, 1, 1, 0, 1],
     [1, 1, 0, 0, 0, 0, 1, 1], [1, 1, 1, 1, 1, 1, 1, 1]],
    # frame 5
    [[1, 1, 1, 1, 1, 1, 1, 1], [1, 0, 0, 1, 1, 0, 0, 1],
     [1, 0, 0, 1, 1, 0, 0, 1], [1, 1, 1, 1, 1, 1, 1, 1],
     [1, 1, 1, 1, 1, 1, 1, 1], [1, 1, 1, 1, 1, 1, 1, 1],
     [1, 0, 0, 0, 0, 0, 0, 1], [1, 1, 1, 1, 1, 1, 1, 1]],
    # frame 6
    [[1, 1, 1, 1, 1, 1, 1, 1], [1, 0, 0, 1, 1, 0, 0, 1],
     [1, 0, 0, 1, 1, 0, 0, 1], [1, 1, 1, 1, 1, 1, 1, 1],
     [1, 1, 1, 0, 0, 1, 1, 1], [1, 1, 0, 1, 1, 0, 1, 1],
     [1, 1, 1, 0, 0, 1, 1, 1], [1, 1, 1, 1, 1, 1, 1, 1]],
    # frame 7
    [[1, 1, 1, 1, 1, 1, 1, 1], [1, 0, 1, 1, 1, 1, 0, 1],
     [0, 0, 0, 1, 1, 0, 0, 0], [1, 0, 1, 1, 1, 1, 0, 1],
     [1, 1, 1, 0, 0, 1, 1, 1], [1, 1, 0, 1, 1, 0, 1, 1],
     [1, 1, 1, 0, 0, 1, 1, 1], [1, 1, 1, 1, 1, 1, 1, 1]],
    # frame 8
    [[1, 1, 1, 1, 1, 1, 1, 1], [1, 1, 1, 1, 1, 1, 1, 1],
     [0, 0, 0, 1, 1, 0, 0, 0], [1, 1, 1, 1, 1, 1, 1, 1],
     [1, 1, 1, 0, 0, 1, 1, 1], [1, 1, 0, 1, 1, 0, 1, 1],
     [1, 1, 1, 0, 0, 1, 1, 1], [1, 1, 1, 1, 1, 1, 1, 1]],
    # frame 9
    [[1, 1, 1, 1, 1, 1, 1, 1], [1, 0, 1, 1, 1, 1, 0, 1],
     [0, 0, 0, 1, 1, 0, 0, 0], [1, 0, 1, 1, 1, 1, 0, 1],
     [1, 1, 1, 0, 0, 1, 1, 1], [1, 1, 0, 1, 1, 0, 1, 1],
     [1, 1, 1, 0, 0, 1, 1, 1], [1, 1, 1, 1, 1, 1, 1, 1]],
]

#
# run until we are out of animation frames
# use Gemma's built-in reset button or switch to restart
#
# populate matrix
while True:

    if frame_count < len(animation) and rep_count >= 0:
        for x in range(x_pix):
            for y in range(y_pix):
                matrix.pixel(x, y, animation[frame_count][x][y])

        # next animation frame
        frame_count += 1

        # show animation
        matrix.show()

        # pause for effect
        time.sleep(frame_delay[frame_count])

    else:

        matrix.fill(0)
        matrix.show()
        time.sleep(.1)

        # track repitions
        rep_count -= 1

        # play it again
        frame_count = 0

        # A0/D1 pin has been touched
        # reset animation
        if touch.value:
            frame_count = 0
            rep_count = reps

View on GitHub

Assembling Circuit

Setting up wires

You will need to cut and strip 6 strands of 30 gauge wrapping wire for connecting the button ‎and 8x8 LED matrix to GEMMA. Measure the length of the strips to about 90mm. You can ‎optionally add labels to each wire with a piece of masking tape. If your new to working with ‎GEMMA, check out the intro guide.‎

Mini 8x8 LED Matrix

The 0.8' led matrix comes with an I2c Backpack that will need to be soldered to the matrix. ‎Carefully slide the matrix into the backpack and flip it over. Triple check that the text is on ‎the same side as the From Adafruit text. Be sure to check out the 8x8 LED matrix intro guide.

Solder all 16 pins. Apply the soldering iron to the pin and hold it there for a few seconds. ‎Add small amount of solder to heated pin, not the tip of the iron! Clip and trim the pins ‎when you're finished soldering.‎

Wiring 8x8 LED Matrix

Apply a small amount of solder to tin the 4 pins on the top of the 8x8 LED matrix backpack. ‎Try to heat the back of the pin and then applying the solder to the front of the pin.

Solder 4 strips of 30 gauge wrapping wire to the 4 pins on the backpack. Try heating the ‎back and pushing the wire through once it's liquidy.‎

3d_printing_matrix-tin_9

3d_printing_matrix-tin_10

Connecting 8x8 LED Matrix to GEMMA

Use a third helping hand to hold your components in place while you solder. Tin the 6 pins ‎on the GEMMA. Solder the 4 wires from the LED Matrix to the pins of the GEMMA. Below is a ‎mini reference list for each pin.

  • SLC to D2/A1‎

  • SDA to D0

  • GND to GND

  • VCC to VBat

3d_printing_gemma-d1_11

3d_printing_gemma-d1_12

3d_printing_matrix-gemma-hero_13

And here's the GEMMA + 8x8 LED matrix circuit! At this point, you can plug in a Lipo battery ‎to the JST to power it on and test if it works. The mini 8x8 LED Matrix should have enough ‎slack to move freely from the GEMMA.‎

3d_printing_power-switch-circuit_14

Switch/JST adapter

For conveniently powering our circuit, we recommend creating a switch/JST adapter. Using ‎a JST extension cable, we can splice it onto a slide switch. The male end of the JST connects ‎to the GEMMA, while the female port connects to your rechargeable battery.

Tin the middle and any outside pin of the slide switch with a small amount of solder. Be ‎sure to apply rosin to each pin in order for the solder to stick properly. Use heat shrink ‎tubing to secure our soldered connections.

Snip off the extra pin in the switch. It could cause a short in our circuit once it's mounted in ‎the box enclosure.‎

Use a third helping hand to assist you. Use ‎each arm to hold onto the JST ports. Use ‎diagonal tweezers to hold the stripped wire ‎with one hand while using your other hand ‎to hold the soldering iron.‎

3d_printing_switch-jst-solder_15

3d_printing_slide-switch_16

Push Button

Use a tactile push button for replaying the LED animations.‎

Snip off any two diagonal pins and tin them.

Before soldering, be sure to add a piece of heat shrink tubing for securing the connection ‎after you solder.

Solder one piece of wrapping wire to each pin.

With the wires securely soldered, put the heat shrink tubing over the connects and heat it up ‎to seal the connections.

Once the button is wired up, solder the two wires to the GEMMA. Order of pins doesn't ‎matter as long as one goes to 3V and the other to D1.

  • Pin A to 3V

  • Pin B to D1‎

pushbutton_17

pushbutton_18

pushbutton_19

pushbutton_20

pushbutton_21

Here's what the complete circuit looks like. The push button should also have enough slack ‎for it to move around in the enclosure. Gemma acts as BMO's brains, while the LED ‎matrix+backpack is his face. We can assume the battery is his heart ;-)

The next page shows you how to put these electro guts into BMO's boxy box.‎

Assembling BMO

assembling_22

Be careful when moving the cables around! Be super cautious not to over flex/bend any of ‎the wires, it could totally break and that sucks! But if any of them do, you can re-solder your ‎connections.‎

Adding the 8x8 LED Matrix

Before adding the LED matrix, add a black piece of tape to cover up the slot right below ‎BMO's face. It's just for decoration; it doesn't actually do anything but adds a great finishing ‎detail to make BMO look more like BMO.

Position the 8x8 LED matrix 'upright' by making sure the pin outs are at the top and Adafruit ‎logo at the bottom. Insert the LED Matrix into box with the top going in first, and then the ‎bottom. The LED matrix should loosely fit into the BMO's box enclosure. Ensure the wiring ‎in the pinout are positioned to the top.‎

3d_printing_bmo-matrix-outside_23

3d_printing_bmo-matrix-outside_24

3d_printing_bmo-matrix-outside_25

Adding Push Button

Gently move the wiring of the LED matrix ‎away from the top clips.

Slightly bend one of the pins of the push ‎button inward, so it does not touch any ‎part of the LED Matrix.

3d_printing_bmo-pushbutton_24

Insert one side of the button into the clips ‎near the top of the box. Align up the push ‎button with the hole in the top middle. ‎Apply pressure to the opposite side of the ‎button while pushing the top of the box ‎inward. This will make a slight bend ‎allowing the push button to snap into ‎place.‎

3d_printing_bmo-button-technique_25

Add Gemma

Place GEMMA over the back of the box ‎cover with the USB port aligned up to the ‎bottom opening. Lightly press GEMMA ‎down into the cover so it stays put.‎

3d_printing_bmo-gemma-cover2_26

Add the JST/Switch adapter to the GEMMA. ‎Make sure two cables are not too long or ‎else it won't fit inside the box!‎

3d_printing_bmo-switch-gemma_27

Closing it Up

You will need to neatly fit the GEMMA, Lipo battery and the JST/switch adapter into the box. ‎For an easier build, try using a 110mAh lithium polymer battery (the 150mAh is a little more ‎tricky to fit into the box, but it can be done!). Place the battery in between the Gemma and ‎led matrix.

If the cover doesn't quite close, you may need to reduce the length of the battery cable ‎and/or the JST/switch adapter. With patience, trial and error, your box will nicely close shut ‎with a little wiggle room.‎

3d_printing_bmo-closing-cover_28

3d_printing_bmo-closing-cover_29

3d_printing_bmo-closing-cover_30

Mounting JST/Switch adapter

Carefully adjust the cables and insert the switch through the cut out near the top of the box ‎cover. If the wires are too long, you may need to cut off some slack, so all the components ‎fit inside the box.‎

3d_printing_bmo-adding-switch_31

3d_printing_bmo-adding-switch_32

Add the Finishing Details

If you have already, pop in the button pieces into the holes on the front of BMO's boxy box. If ‎they don't fit, using an x-acto knife to loosen up the opening. Be careful, don't over loosen ‎the holes or the limbs and buttons won't stay put! But if you do, you can super glue them ‎into place. BMO's arms and legs should freely rotate.

‎Add a split ring to the cover and put it on a necklace to wear your new electronic pal for a 3d ‎printed adventure time!‎

3d_printing_bmo-buttons_33

3d_printing_bmo-buttons_34

3d_printing_bmo-buttons_35

3d_printing_hero3

Codice produttore 57818
WIRE STRIPPERS & CUTTERS 7.25"
Wiha
Codice produttore 1446
WIRE WRAP THIN PROTOTYPING & REP
Adafruit Industries LLC
Codice produttore 3501
ADAFRUIT GEMMA M0 - MINIATURE WE
Adafruit Industries LLC
Codice produttore 1222
WEARABLE PLATFORM GEMMA V2 MINI
Adafruit Industries LLC
IC SOCKET - FOR 20-PIN 0.3 CHIPS
Codice produttore 2204
IC SOCKET - FOR 20-PIN 0.3 CHIPS
Adafruit Industries LLC
Codice produttore 291
MAGNIFIER STAND 2.5" 4X
Adafruit Industries LLC
Codice produttore 422
TWEEZERS POINTED FINE 4.72"
Adafruit Industries LLC
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.