Maker.io main logo

Display Temperature & Humidity Using ATOM Matrix ESP32 and DHT11 Sensor

2026-05-22 | By Ron Cutts

License: GNU Lesser General Public License Displays Microcontrollers Wifi Arduino ESP32

In this tutorial, we are going to display temperature and humidity from the DHT11 sensor using the ATOM Matrix ESP32. Values will be displayed proportionally according to the matrix display.

Learn more about Visuino: What is Visuino

What You Will Need

What You Will Need

What You Will Need photo 2

What You Will Need photo 3

What You Will Need photo 4

The Circuit

  • Connect DHT11 sensor pin [VCC] to Atom Matrix pin [5V]

  • Connect DHT11 sensor pin [GND] to Atom Matrix pin [GND]

  • Connect DHT11 sensor pin [S] to Atom Matrix pin [G25]

The Circuit

Start Visuino, and Select the Atom Matrix Board Type

Start Visuino as shown in the first picture. Click on the "Tools" button on the Arduino component (Picture 1) in Visuino. When the dialog appears, select "Atom Matrix" as shown in Picture 2

Start Visuino, and Select the Atom Matrix Board Type

Start Visuino, and Select the Atom Matrix Board Type photo 2

In Visuino, Add Components

  • Add "DHT11" sensor component

  • Add 2X "Map Range Analog" component

  • Add 2X "Analog To Integer" component

  • Add 2X "Integer Multi Source" component

In Visuino Add Components

In Visuino Add Components photo 2

In Visuino Add Components photo 3

In Visuino Add Components photo 4

In Visuino Set Components

  • Select "M5 Stack ATOM Matrix" board, and in the properties window, expand "Modules">"RGB Matrix">"Elements" and click on the 3 dots button

  • In the "Elements" window, drag "Draw Rectangle" to the left side and in the properties window select "Height" and click on the Pin Icon and select "Cardinal SinkPin", set the "Color" to aclGreen, "Width" to 2, "Height" to 0

  • In the "Elements" window, drag another "Draw Rectangle" to the left side, and in the properties window select "Height" and click on the Pin Icon and select "Cardinal SinkPin", set the "Color" to $FF0080FF , "Width" to 2, "Height" to 0, "X" to 3

  • Close the "Elements" window

We need to adjust the values from the DHT11 sensor to the matrix display. To do that:

  • For the Temperature: Select "MapRange1" and in the properties window set "Input Range" > "Max" to 35 and "Output Range" > "Max" to 4

  • For the Humidity: Select "MapRange2" and in the properties window, set "Input Range" > "Max" to 100 and "Output Range" > "Max" to 4

In Visuino Set Components

In Visuino Set Components photo 2

In Visuino Set Components photo 3

In Visuino Set Components photo 4

In Visuino Set Components photo 5

In Visuino Set Components photo 6

In Visuino Set Components photo 7

In Visuino Set Components photo 8

In Visuino Connect Components

  • Connect "HumidityThermometer1" pin [Sensor] to "M5 Stack ATOM Matrix" pin [GPIO 25]

  • Connect "HumidityThermometer1" pin [Temperature] to "MapRange1" Pin [In]

  • Connect "HumidityThermometer1" pin [Humidity] to "MapRange2" Pin [In]

  • Connect "MapRange1" Pin [Out] to "AnalogToInteger1" pin [In]

  • Connect "MapRange2" Pin [Out] to "AnalogToInteger2" pin [In]

  • Connect "AnalogToInteger1" Pin [Out] to "IntegerMultiSource1" pin [In]

  • Connect "AnalogToInteger2" Pin [Out] to "IntegerMultiSource2" pin [In]

  • Connect "IntegerMultiSource1" Pin [0] to "M5 Stack ATOM Matrix" > "Draw Rectangle1" pin [Height]

  • Connect "IntegerMultiSource1" Pin [1] to "M5 Stack ATOM Matrix" > "Draw Rectangle1" pin [Clock]

  • Connect "IntegerMultiSource2" Pin [0] to "M5 Stack ATOM Matrix" > "Draw Rectangle2" pin [Height]

  • Connect "IntegerMultiSource2" Pin [1] to "M5 Stack ATOM Matrix" > "Draw Rectangle2" pin [Clock]

In Visuino Connect Components

In Visuino Connect Components photo 2

Generate, Compile, and Upload the Arduino Code

In Visuino, at the bottom, click on the "Build" tab, make sure the correct port is selected, then click on the "Compile/Build and Upload" button.

Generate, Compile, and Upload the Arduino Code

Play

If you power the ATOM Matrix module, the display will start to show the temperature as green and humidity as blue. Values are proportional according to the ATOM Matrix display size.

Congratulations! You have completed your project with Visuino. Also attached is the Visuino project that I created for this tutorial; you can download it and open it in Visuino: https://www.visuino.eu

Downloads

Codice produttore C008-B
ATOM MATRIX ESP32 EVAL BRD
M5Stack Technology Co., Ltd.
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.