Using the voltage program feature, the output voltage of the GWS500 can be adjusted over a wide range, as shown here in the slide. The bottom right hand graph shows the external voltage level required to program the output. To set the output voltage of the GWS500-24 to 28.8V for example, apply 6V to the "PV" terminal.