Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List
Phase-Slide10

This graphic shows the potential air gaps that exist between the device and the heatsink, which were covered in the previous slide. These gaps must be controlled by using the correct interface material. When both a heatsink and device are both flat and smooth, a thin TIM such as grease or phase change may be used. If the devices are not coplanar by a large amount, a gap filler material may be a better choice.

PTM Veröffentlicht am: