Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List
Phase-Slide16

This slide shows a case study of four different TIMs on the same device. The device is a common size and power for the electronics industry. By changing from a high performance tape to a phase change material, the device temperature can be reduced by 22.4°C. This temperature reduction is from changing the TIM only, as the heatsink is identical. The benefits of using a phase change material, in conjunction with a clip-on attachment, are clearly shown.

PTM Veröffentlicht am: