Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List
Phase-Slide8

Thermal conductivity is the ability of a material to conduct heat after it has entered that material. Thermal conductivity values can be misleading when used to evaluate thermal interface materials since actual performance is affected by the contact resistance with both the heatsink and the processor. In later slides the effect of conductivity on actual performance will be shown.

PTM Veröffentlicht am: