Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List
Phase-Slide11

In this slide, the effects of uneven components are shown. In the first example, a concave device makes contact with the TIM only at the edges. This is an example of the TIM not filling the interfacial gap correctly. In the second example the component heat spreader has a convex bump on the center. This allows for contact in the center of the package above the die. Applying ink to a component before attaching a taped on heat sink is a good diagnostic tool to ensure correct contact.

PTM Veröffentlicht am: