Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List
Phase-Slide12

Thermal impedance is the measure of the interfacial resistance of a TIM, its conductivity, and the TIM thickness. It is calculated by dividing the temperature difference across the interface, per unit area, by the power output of the processor. Thermal impedance is expressed in units of °C-in2/W and must be used with effective contact area.

PTM Veröffentlicht am: