Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Product List
OpAmp-Slide14

Temperature drift can affect many DC parameters. Three specifications that will change over temperature are offset voltage, gain, and bias current. The datasheet will show typical and maximum values for how a device will perform over temperature. These graphs are from the OP07D, a very low cost precision op amp. The first graph is a histogram that shows the number of amplifiers with different values of temperature drift. The specifications in the datasheet show a maximum of 1.5uV/°C change, and a typical 0.5uV/°C drift. Most op amps have less than 0.5uV/°C of drift. The second graph shows how the total offset voltage will change over a temperature range.

PTM Veröffentlicht am: