Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Product List
OpAmp-Slide40

Another important attribute is if the amplifier offers “rail-to-rail” performance. Amplifiers typically have a certain amount of headroom on the inputs and outputs. For instance, if an op amp operates from a +/- 5V supply, its input and output signals maybe restricted to a maximum of +/- 4V.  So the full range of the power supply rails are not used. A rail-to-rail amplifier can accept inputs and generate output voltages very close to the power supply rails.

PTM Veröffentlicht am: