Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Product List
OpAmp-Slide38

Crosstalk is a concern when multiple op amps are in one package. Information from one channel should not leak directly into the other channel. This is typically specified in dB (like CMRR or PSRR) and is a measure of how well each amplifier is isolated from the other amplifiers in the package. Like CMRR and PSRR, crosstalk depends on the frequency of the signals.

PTM Veröffentlicht am: