Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Product List
OpAmp-Slide5

A voltage feedback op amp responds to a voltage difference between the inputs, while a current feedback op amp responds to a current difference between the inputs. Both inputs on a voltage feedback op amp are high impedance. In a current feedback op amp, the non-inverting input has a high impedance while the inverting input has a low impedance. Voltage feedback op amps also have a constant gain bandwidth product, which means if an op amp’s BW is 100MHz at a gain of 2, the gain BW product is 200MHz.

PTM Veröffentlicht am: