Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Product List
OpAmp-Slide2

Amplifiers can be used for many applications, but their primary use is to simply increase the amplitude of an AC or DC signal. They can also be used to buffer signals. Amplifiers have high input impedance and low output impedance, which means they do not load a source (like a sensor) and can drive a changing load. One application for this is in driving ADCs. When an ADC is sampling the input signal the input impedance changes. This changing impedance can affect the accuracy of a sensor.  By using an amplifier, the accuracy of a sensor can be preserved.

PTM Veröffentlicht am: