Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
MLPMLS-Slide12

Shown here is the edge view of the thermal profile. The temperature rise at the hotspot is 13.7°C. That is a thermal resistance of 2.7°C/W. While that is about the same as a snap-in capacitor’s hotspot-to-case thermal resistance, a snap-in’s hotspot to ambient thermal resistance would be about 7.3°C/W approaching three times the temperature rise. The easy ability to heatsink the MLP and MLS assure easy cooling and long life with high ripple currents.

PTM Veröffentlicht am: