Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
MLPMLS-Slide16

MLP and MLS capacitors rated at 250V and less have great cold temperature capability. These typical curves show more than 90% of the capacitance is retained at –55°C at the standard test frequency of 120Hz. It is even better at lower frequencies but falls off at higher frequencies.

PTM Veröffentlicht am: