Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
MLPMLS-Slide13

Shown here is the MLP is standing on edge and one of its small sides is held at 65°C. The hottest spot on the opposite small side with 5W of power is only 3°C hotter, and that is a thermal resistance of 0.60°C/W, only two thirds more than with the bottom heatsunk. This shows that MLP and MLS flatpack capacitors are easy to heatsink.

PTM Veröffentlicht am: