Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Product List
MLPMLS-Slide19

Continuing the comparison of the MLP’s cold temperature performance to a same-rating snap-in capacitor, the red curves are ESR and the purple curves are capacitance. At 1000Hz and –40°C the snap-in’s ESR has increased 49.3 times while the MLP’s ESR has increased only 7.4 times. The snap-in’s capacitance is down to only 40% while the MLP’s is at 82% of the room temperature value.

PTM Veröffentlicht am: