Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25
How An Encoder Functions

Inside a rotary encoder there is a disc, fixed to a shaft that is free to rotate. On one side of the disc is a signal source, on the other side a receiver. As the disc turns, the signal source is alternately allowed to pass and be blocked. When the signal is passed through the disc, an output pulse is generated. In the illustration here, signal A passes through the disc generating an output pulse. At the same time signal B is blocked and no output pulse is generated. The dotted line represents the position of the disc relative to the output pulses.

PTM Veröffentlicht am: