Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Product List
EST-Slide17

As load levels increase, switch life decreases. However, the rated current is only one point on a curve of switch life versus electrical load. For example, a switch having a current rating of 15A at 125VAC in room conditions, based on a life of 100,000 operations with 95% survival, can be expected to satisfactorily control currents below 15A. This life-vs.-load chart for the switch at these conditions shows the expected life at currents below the rated load. At each condition for which the switch is rated, the switch can close the circuit, carry the steady-state current indefinitely, and open the circuit during each cycle of operation through its life.

PTM Veröffentlicht am: