Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Product List
EST-Slide20

In other applications such as high-flying aircraft, as atmospheric pressure is reduced, an unsealed switch will experience an increase in arc energy and a slight reduction of dielectric properties. Under some conditions, it may be necessary to reduce the current rating to maintain the same switch life. Shock and vibration are also variables that can impact switch performance. To help assure adequate switch life, it is wise to test the switch under conditions simulating those of the actual application environment.

PTM Veröffentlicht am: