Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Product List
EST-Slide27

The parameters to review for actuation include pre-travel, over and differential travel, operating force, and release force. Pretravel is the distance the actuator plunger must move from free position to operating position and overtravel is the distance it moves past the actual operating point. Differential travel is the distance from operating point to release point. Operating force is the amount of force that must be applied to the plunger to cause the switch to actuate. Release force is the level to which force on the plunger must be reduced to allow it to snap back. These are important parameters to understand when specifying what the switch must do, and therefore ultimately the type of switch to use.

PTM Veröffentlicht am: