Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Product List
Charge Pump

FETS are difficult to operate at low voltages. They may not turn on or off reliably if the gate cannot be biased high enough. Many applications in mobile phones need to operate at only a few volts, right near the lower limit of the FET. To make the load switch work reliably at this low voltage, a charge pump can be added to boost the gate voltage internally to the proper levels.

PTM Veröffentlicht am: