Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
USB-Continuum-slide12

Here is an operator interface example based on MCF5227x. The highly integrated devices combine both on-chip color LCD and touch-screen controllers to enable touch-based user interfaces. The operator interface can monitor, control, and display on one interface. The system bus controller can be used to communicate with external systems and memory. The integrated peripherals such as USB, LCD, and CAN help reduce system cost greatly and ease the development process.

PTM Veröffentlicht am: