Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
USB-Continuum-slide5

The MC9S08JM16 (JM16) family based on the S08 core further extends the low end 8-bit USB solutions in NXP USB controller continuum. The JM16 features up to 16KB of flash memory, a full speed USB device and a 12-channel, 12-bit analog-to-digital converter. It also has several system protection features such as low voltage detect and a Computer Operating Properly (COP) module.

PTM Veröffentlicht am: