Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Product List
USB-Continuum-slide16

The USB-LITE Stack by CMX provides USB host and device function which supports the 8-bit and 32-bit embedded USB controllers. It supports HID class in host and device mode, CDC to UART, and mass storage function in host mode. The USB-MINI Stack is developed by NXP with a USB device driver for the 8-bit JM family. It’s highly optimized for the smallest footprint 8-bit family devices. Users can also define their own high-level class protocol base on USB-MINI stack for flexible customization.

PTM Veröffentlicht am: