Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Product List
LinkSwitch-II Overview Slide 11

PI Expert is an interactive program that takes a user's power supply specifications and automatically determines the components needed to generate a working switch mode power supply. This program can also optimize designs for cost and efficiency while it dramatically reduces design time. As shown in the slide, the new PI-XLS “LinkSwitch-II Flyback Design” file type displays data in a spreadsheet which allows parameters to be easily adjusted. For example, if the maximum computed duty cycle exceeds 55% the input capacitance can be increased by simply entering a new value.

PTM Veröffentlicht am: