Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Product List
LinkSwitch-II Overview Slide 5

As shown in the figure, the no-load power consumption increases with the input voltage but remains less than 200 mW. However, when an external bias circuit is implemented, the no-load input power remains close to 25 mW as the input voltage is increased. These are both well below the 300 mW CEC/Energy Star 2.0 limit.

PTM Veröffentlicht am: